Other Parts Discussed in Thread: CC-ANTENNA-DK2, CC110L, CC115L, CC1310
I am designing a circuit with CC1350, with 868MHz as the operating frequency. There are a lot of good application / design notes and antenna selection guide, which I have gone though. Before I can make a choice, I need some help.
The preferred antenna is the helical loop antenna, which is used in CC1350 Launch Pad (swrc320a), and in CC115L/CC110L Value Line Reference Design (swrr082a). It is documented in DN038 (swra416) and CC-Antenna-DK2 (swra496a).
Questions:
1. The reference RF differential circuit between the CC1350 and the antenna matching circuit is available in CC115L/CC110L Reference Design schematic, and in Section 3.1 of the Application Note "CC13xx/CC26xx Hardware Configuration and PCB Design Considerations" (swra640g). These are not identical. So, is either circuit okay to use? Or is one of them more advisable? Is this reference circuit same 868 MHz operation with these devices - CC1310, CC110, CC115, CC1350?
2. Assuming that helical antenna reference given in CC115L/CC110L Value Line Reference Design (swrr082a) is the correct choice, then is it okay to reduce the width of the board from 40mm to 22mm (slightly higher than the width of the helical antenna)? The idea is to keep design small. The ground plane will still have the same length. Is this approach okay?
3. The documentation says in some places that 4-layer PCB is preferred for 868MHz antenna designs for sub-GHz devices. However, the gerber files for the CC115L/CC110L Value Line Reference Design (swrr082a) only have two layers, and the board is 0.8mm thick. Is this is a good reference to follow for CC1350 PCB design?
4. The CC1350 Launch Pad is 4-layer and 1.6mm thick. If this launchpad is a better design to refer to, then, is it okay to keep the ground plane to about 25x25mm? If the ground plane is reduced in area, then could you please give a suggestion for approximate increase in the design length of the helical antenna (so that it can be cut to size after the board is back)?
5. Is it completely impossible or not advisable to design the helical antenna in a 2-layer and 1.6mm board? If so, please advise on the reference design to follow.
Thank you!
Regards, Maneesh