This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1120: cc1120 & cc debug

Part Number: CC1120
Other Parts Discussed in Thread: CC-DEBUGGER

HI~

I have a question when connecting CC1120 to cc debug.

The DC/DD waveform was measured during the RF test by performing SMARTRF STUDIO by connecting CC1120 to cc debug.

1) Both DC/DD are low for the continuous test, and DC LOW and DC HIGH for the packet test. What is the reason?

2) Under what conditions does DC/DD operate with DATA and CLOCK?

3) When CC1120 and CC DEBUG are connected, what are the errors if DC/DD are not connected?

4) What role does DC/DD play when CC1120 and CC DEBUG are connected?

Best Regards,

KWON.