Part Number: CC1312R
Other Parts Discussed in Thread: CC1352R, , CC1260
Hi!
We are checking the capabilities of the transmitter of the TI CC1312R and TI CC1352R modules in the band 861-1054 MHz.
This is a band with available bandwidth 193 MHz to be used by the transmitter. If I have multiple TICC1312R transmitting at the same time, and I am using the Non-Orthogonal Multiple Access (NOMA) technique, there will be interference sensed at the receiver. In the case that I would like to use the Orthogonal Frequency Division Multiple Access (OFDMA) technique, am I able with this wireless module to subdivide the 193 MHz available bandwidth to subchannels and allocate the subchannels to the transmitters in order to decrease the interference? If yes, what is the length of each subchannel in MHz or KHz, what is the guarding space between adjacent subchannels, and how many subchannels are available?
Are the TI CC1312R and TI CC1352R modules reprogrammable to allow me to allocate dynamically the aforementioned subchannels to different transmitters, so they solely transmit to the specific subchannel. My experiment is mainly focusing on dynamic bandwidth allocation in NOMA and OFDMA multiple access communication environments.