Other Parts Discussed in Thread: CC1190, CC1120
hello. Experts
I previously received a lot of help from TI Froum in transmitting/receiving coding related to cc1120.
I'm working on another RF-related project and I had a question, so I decided to write this post.
I am conducting wireless communication between my radio and BOOSTXL-CC1120-90.
Please refer to the picture below

The transmitting and receiving frequencies are set to be the same.
However, the moment the radio transmits a packet, a communication error is displayed on Smart RF as shown below, and the connection between the PC and BOOSTXL-CC1120-90 is lost.

Even after checking the BOOSTXL-CC1120-90 manual, I do not know why this phenomenon occurs.
Transmission and reception are working well with the module that was previously tested with BOOSTXL-CC1120-90.
If you know the reason or cause of this problem, I would greatly appreciate your help.
Thankyou for reading
- Kim -