I am currently using a SmartRF05EB Rev 1.8.1 and trying to connect to SmartRF Studio 7 Rev I. I installed the Cebal and connected it through the CC2531 USB Dongle. For the life of me I can't get the device to connect up, however everything works 100% when running the demo temperature program that comes pre-installed. I am connecting the Dongle to the Debugger. I am lost. If there is anything that I need to check I would be extremely appreciative if someone would give me a heads up. Thanks,
Andrew