Other Parts Discussed in Thread: CC1101
Greetings forum!
We are experiencing a peculiar behavior that we are not able to corelate with theoretical or expected outcome on CC1310. We are testing the ability of the device to withstand crystal drift by streching to its limits. The test setup and radio settings are elaborated below:
1.The radio configuration is legacy long range mode with DSSS=1 at 70kbps symbol rate and 35KHz deviation and Fc at 868MHz.
2. The crystal in use has an accuracy of +-10PPM on both Tx and Rx,as per Design Note DN005, titled CC11xx Sensitivity Versus Frequency Offset and Crystal Accuracy, the compensation for crystal inaccuracies is given by the 4*XTAL ppm i-e, 4*8.68Khz,34.72KHz.So the required receiver filter bandwidth becomes=2*70KHz+34.72KHz=174.72KHz. This effective signal bandwidth is easily catered by Rx filter bandwidth of 196KHz at the receiver.
3. With radio link established and working fine, we begin to change the receiver Fc from 868 MHz in steps of 1KHz. It is at 868.030 MHz, a crystal drift of 30KHz, when the link is compromised and everything goes blank at the receiver. At this point.
4. If our mathematics is correct, there is now a need for a Rx filter bandwidth of 174.72+30=204.72Khz to receive the complete channel bandwidh, so we proceeded to change the Rx filter bandwith from 196KHz to 255KHz only to find out that there was no link availability. But as soon as we increase the Rx filter bandwidth to 311KHz, the next programmable step for Rx filter bandwidth, the link is established again smoothly.
We are unable to fathom that why an effective signal bandwidth of 204.72KHz is not completely received within the 255KHz BW of the receive filter?
Please guide me through this query as we are not able to explain this behaviour.
Best Regards
Maaz Ali