I am using the CC1111Fx for academic research and am trying to increase the output power beyond 10dBm without using any external hardware. To get specific measurements, I am deliberately trying to induce distortion of the output signal by saturating the power amplifier.
Referring to datasheet sections 13.15 and Table 72: In the 433 MHz band, I see a positive correlation between PA_TABLE settings and output power. However, the corresponding entry for 10 dBm is 0xC0 while for 7 dBm it is 0xC8. Because of this, I am unsure exactly what the relationship is.
What will a setting like 0xFF or 0xF0 do?