This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 have some question about RF PHY in 4mbps 8-fsk HS mode

Part Number: CC1310


1. CC1310 how to know the RF recive bandwith and frequency deviation in HSM?

2.whether there have a method can change some parameter ,such as rewrite the HWREG value?

3.if there has a register list to interpret every number means in the pOverrides_hsm ?

// Overrides for CMD_RADIO_SETUP HSM
uint32_t shapeovr[] = {0x00000000, 0x00000000, 0x00000000, 0x12010000, 0x72685C43, 0x8986817A};

uint32_t pOverrides_hsm[] =
{
MCE_RFE_OVERRIDE(1,0,0,1,0,0),
ADI_HALFREG_OVERRIDE(0,61,0xF,0x0),
ADI_REG_OVERRIDE(1,4,0x9F),
ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
HW_REG_OVERRIDE(0x4038,0x003A),
HW_REG_OVERRIDE(0x4020,0x7F00),
HW_REG_OVERRIDE(0x4064,0x0040),
0x000604A3,
0xB1070503,
0x05330523,
0x0A480583,
0x7AB80603,
0x00108463,
0x02010403,
0x04B00243,
0x00038883,
0xC0040031,
(uint32_t) &shapeovr[0],
0xC0040021,
(uint32_t) (0x00000035),
0x000388A3,
HW_REG_OVERRIDE(0x50B4,0x6666),
HW_REG_OVERRIDE(0x50B8,0x000C),
(uint32_t)0xFFFFFFFF,
};