This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: How the power configuration is selected

Part Number: CC1310


Hi team

In the TI brochure, I find that there is a statement that the DCDC is less than the global LDO, 433 mode, Tx maximum output power by 1 dBm. 

However, in the manual it is also said that DCDC mode is less power than global LDO. 

Now the problem is, I want to transmit more, less power, at maximum Tx power, How do I choose? 

Best regards

Alex

  • Hi Alex,

    The DC/DC converter does not need to be enabled when using Boost mode, but is more efficient than the global LDO mode. Without Boost mode the maximum output power possible is less and if the +14 dBm setting is selected without Boost mode it will likely output less than +14 dBm.

    So if you want the maximum output power setting then the recommended configuration is: DC/DC enabled, Boost mode enabled, +14 dBm setting.

    Please see Section 11 of SWRA640 (CC13xx/CC26xx Hardware Configuration and PCB Design Considerations): https://www.ti.com/lit/swra640 for information on the different CC13xx power supply configurations.

    To evaluate this, in SmartRF Studio the user can select (or deselect) "DC/DC Enable" and adjust the "TX Power" setting as desired:

    Regards,

    Zack

  • Is there a conflict between enabling boost mode and enabling DCDC mode? 

  • No, not enabling the DC/DC converter will only reduce the efficiency. BOOST mode will work with either DC/DC converter or global LDO mode.

    You will probably not be able to transmit the full +14 dBm without BOOST mode enabled.

    Regards,

    Zack