This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: SubGHz Beacon

Part Number: CC1352R


Dear Sir/Madam,

Can I check does Ti has any reference design for SubGhz beacon application. The concept of working is for smart lightin control application with following spec:

  • Advertisement feature on Sub GHz
  • Operation Range is 2KM.
  • Comply with US Sub GHz frequency brand (868MHz)
  • No Back up batter power
  • Latency is 1 second
  • Data transfer is 30 bytes.

The top level concept block as follow:

If you can guide me to github example or provide any reference design and recommend a eval kit to kick start with, it will be helpful. 

Thx

best regards, Felix

  • Hi Felix,

    a few questions:

    in your application would there be multiple devices communicating to the sub-GHz device that is connected to the gateway (point-to-multipoint)?

    You would need to transmit data bidirectionally, correct?

    By advertisement feature do you mean that you would like to implement and advertisement feature similar to BLE?

    For the US frequency band you actually mean 915 MHz, correct?