Other Parts Discussed in Thread: BLE-STACK,
Hi,
Following is copied from related thread.
Where can we get header from "Each header contains a pointer/address to the actual image".
Regards
"Hi Dong,
Are you using the default ti external flash interface and OAD application?
In the ti example and the figure you posted, external flash starts (address 0x00000000) with the efl headers. Each header contains a pointer/address to the actual image. So the application/BIM can go through all the headers and map out which addresses are occupiied ad which are free.
Cheers,
Marie H"