HI folks,
i try to find something about the calibration time for continuous RX (RX>RX). I try to measure the RSSI values continuous without any IDLE time, but with channel switching.
*So i have to do a calibration after a channel switching?
In DN508 is written that i have to perform a calibration just every 2 MHz., when i switch between the channels.
**When i dont performe a calibration which failure i can expect? I have no idea.
Thanks,
F. Hof