This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101: 433MHz evaluation board

Part Number: CC1101


Hi Team,

Customer is planning on using CC1101 on the receiver side.

Is there an EVM for 433MHz for evaluation purposes?

BR,
Stefan

  • Hi Stefan,

    There is a 433 MHz design for the CC1101:

    CC1101EM434MHz (SWRR046): https://www.ti.com/lit/zip/swrr046

    We currently are "in-between" CC1101 EVMs, where our existing boards are discontinued (and are no longer available on TI.com), but we have not yet finalised a replacement.

    If the expected volumes are high, please contact me directly (or via PM on E2E) to see if we can find a solution, otherwise the customer has two options:

    • Buy from a third party in the interim.
    • Produce their own EVMs using the reference design linked above.

    We can of course provide support on E2E as well.

    Regards,

    Zack