Hi team,
May I know the value of the local frequency of receiver's mixer? From the datasheet, there is a local oscillator 7in the block diagram, and the image frequency can be an issue.
Best regards,
Shunsuke Yamamoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
May I know the value of the local frequency of receiver's mixer? From the datasheet, there is a local oscillator 7in the block diagram, and the image frequency can be an issue.
Best regards,
Shunsuke Yamamoto
Hi Diego,
Thank you so much for your reply. I have listed the answers.
RF frequency: 1216MHz, 1216.5MHz, 1217MHz, 1252MHz, 1252,5MHz, 1253MHz
PHY: CC1312
Best regards,
Shunsuke Yamamoto
Hi Shunsuke,
By PHY I meant the RF physical layer. For the CC1312 we have multiple PHYs that have been characterized with different data rates to transmit/receive the data.
Reduced list from SmartRF studio:

The intermediate frequency can change depending on the PHY used. Which PHY or PHYs would be used?
For the IF frequency, see chapter 10 in https://www.ti.com/lit/an/swra682/swra682.pdf. This also point to the relevant table in the TRM.
Hi Diego-san,
PHY: Narrowband 4.8 kbps, 2 kHz Deviation, 2-GFSK, 10.1 KHz RX Bandwidth.

Best regards,
Shunsuke Yamamoto
The PHY has an intermediate frequency of about 390 kHz. Therefore for the frequencies you listed LO would be at 1215.61 MHz, 1216.11 MHz, 1216.61 MHz, 1251.61 MHz, 1,252.11 MHz, and 1252.61 MHz