This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am inquiring about the possibility of configuring the CC1352 in the following two modes.
1. Direct access to framed data before being modulated via an internal register, programming command, or output to a pin in a test mode, etc.
2. CC13x2, CC26x2 SimpleLink Wireless MCU Technical Reference Manual, Pg 2145, CMD_PROP_RADIO_SETUP modulation indicates "Others: Reserved". Is OOK an available modulation?
Thanks,
Mike
Hi Mike,
2. I would recommend using SmartRF Studio to find settings and check which modulations are available. (If there are no settings for you modulation in SmartRF Studio we don't support it.)
We have one OOK PHY in Studio, does it fit?
Cheers,
Marie H
For 1, can you use MCE_GPO0 described in table 9 in dev.ti.com/.../signal-routing.html