Other Parts Discussed in Thread: CC1120, , CC1311R3, CC1310
Hello,
working with CC112x since many years, now we do have the need of a low cost TX chip, which works with CR2032 coin cells in a keyfob (large volume).
The main application will work with FSK and appr. 20ms packet length (as we need to provide an MCU anyway, we can do packeting by bit-bang, if the chip doesn't provide a packet engine), receiver is a CC1120 in packet mode. (Another -legacy- mode will be ASK with >100ms packet length, legacy receiver. We expect much less current consumption in ASK, so if it fits for FSK 20ms it should also fit for this ASK mode).
Operation is under ETSI EN regulations, so it needs to meet all the OOB and harmonics limitations.
CC115L would fit, but (as usual with all CC's < CC13xx) we do have a current issue: minimum current of all CC11x is ~25mA for a few dBm PA plus the MCU.
The coin cell can't deliver more than 15mA (short term only)- with a simple cap one can't mitigate. And a buck isn't possible due to budget.
Thanks in advance for advice!