This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: The flash write value of CC1310 is incorrect

Part Number: CC1310


Experts , in the use of CC1310 chip, there are the following problems, expect to write 0x00D2, but the actual write value becomes 0x04D2, this is just one example, there are some values also written wrong, basically a certain 1 was not set to 0, what will happen in this situation. And how to avoid this situation. 

  • I am afraid you need to provide more details for use to understand what you are trying to do and how it is failing.

    What SDK version are you using?

    Which HW are you running on (LP or custom HW)

    Which code example from the SDK are you running

    What are the steps we need to do to recreate the issue you are seeing?

    Siri

  • sdk_4_20_02_07

    HW base on custom HW

    just use the sdk low_level_driver

    This situation generally occurs in the case of battery power, the battery voltage is about 2.9V, and the current limit is 50ma,power mode is LDO

  • You have still not provided info that makes us able to try to reproduce that you are seeing.

    You have custom HW that we do not know anything about, and are using low lever drivers.

    If you want us to look into this you need to provide code that runs on a LP so that we can reproduce the issue here.

    Siri