Part Number: CC430F5137
Other Parts Discussed in Thread: TEST2, CC1101
We are a data company based out of the UK who use a data collection device which utilises RF transmission. The device is an instrumented mouthguard which transmits data using an ST Electronics low powered transceiver component. During use, this RF transmission is captured by a receiver plugged into a PC nearby.
This set up is certified for FCC and CE, with the caveat that during compliance testing, the frequency band had to be made wider for the FCC regulations:
|
|
CE |
FCC |
|
Base Frequency |
868 MHz |
921 MHz |
|
Frequency Deviation |
20 kHz |
229 kHz |
|
Channel Bandwidth |
100 kHz |
541 kHz |
In the past we have used an ST chip on the RX side, however, we have now switched to using the CC430F5137 by Texas Instruments.
Using our CE settings, the transition has been seamless, and the performance is almost identical to what was achieved with the ST chip. However, in the US where we use the FCC settings, the range at which the product can work has decreased massively. The table below displays this.
|
|
CE |
FCC |
|
ST CHIP |
100m range |
100m range |
|
TI CHIP |
100m range |
5m range |
Last time I asked about this, I was pointed towards the SmartRF studio.
Below is a table containing our CE register settings (good range), our FCC register settings (bad range), and RF studio recommended settings for FCC.
|
Register Setting |
CE Settings |
FCC Settings |
RF Studio FCC |
|
IOCFG1 |
0x09 |
0x09 |
0x09 |
|
IOCFG0 |
0x06 |
0x06 |
0x06 |
|
PKTLEN |
0x3D |
0x3D |
0x3D |
|
PKTCTRL1 |
0x06 |
0x06 |
0x06 |
|
PKTCTRL0 |
0x05 |
0x05 |
0x05 |
|
ADDR |
0x01 |
0x01 |
0xAA |
|
CHANNR |
0x01 |
0x02 |
0x02 |
|
FSCRTL1 |
0x0C |
0x0C |
0x0C |
|
FREQ2 |
0x21 |
0x23 |
0x23 |
|
FREQ1 |
0x62 |
0x6C |
0x6C |
|
FREQ0 |
0x76 |
0x4E |
0x4E |
|
MDMCFG4 |
0xCA |
0x2A |
0x2A |
|
MDMCFG3 |
0x83 |
0x83 |
0x83 |
|
MDMCFG2 |
0x13 |
0x13 |
0x13 |
|
DEVIATN |
0x35 |
0x71 |
0x71 |
|
MCSM0 |
0x10 |
0x10 |
0x10 |
|
F0CCFG |
0x16 |
0x16 |
0x16 |
|
AGCCTRL2 |
0x43 |
0x43 |
0x43 |
|
WORCTRL |
0xF0 |
0xF0 |
0xFB |
|
FSCAL3 |
0xE9 |
0xE9 |
0xE9 |
|
FSCAL2 |
0x2A |
0x2A |
0x2A |
|
FSCAL1 |
0x00 |
0x00 |
0x00 |
|
FSCAL0 |
0x1F |
0x1F |
0x1F |
|
TEST2 |
0x81 |
0x81 |
0x81 |
|
TEST1 |
0x35 |
0x35 |
0x35 |
|
TEST0 |
0x09 |
0x09 |
0x09 |
|
BSCFG |
0x6C |
0x6C |
Not present |
|
MCSM1 |
0x30 |
0x30 |
Not present |
|
FSTEST |
0x59 |
0x59 |
Not present |
|
F1F0THR |
0x07 |
0x07 |
Not present |
|
IOCFG2 |
0x29 |
0x29 |
Not present |
|
FREND1 |
0x56 |
0x56 |
Not present |
|
FREND0 |
0x10 |
0x10 |
Not present |
|
AGCCTRL1 |
0x40 |
0x40 |
Not present |
|
AGCCTRL0 |
0x91 |
0x91 |
Not present |
|
MDMCFG1 |
0x22 |
0x22 |
Not present |
|
MDMCFG0 |
0xF8 |
0xF8 |
Not present |
|
FSCTRL1 |
0x08 |
0x0C |
Not present |
|
FSCTRL0 |
0x00 |
0x00 |
Not present |
From these settings I can't see anything that should be resulting in the decreased performance.