Hi Champs,
There is some use cases that the router nodes (RNs) are not powered all the time, but only the Border Router (BR). There are maximum 200 RNs per PAN.
Let's say after the network is completely formed, ie. 100% of the nodes successfully join the network, then the RNs are powered off for some time. So, is there a method to reduce the join delay to a minute or two when all the RNs are powered up again in FAN1.0? If FAN1.1 can do, pls advise too.
Regards,
Kien Nguyen