This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-XDS110ET: Looking to build 20-Pin to 14-Pin Adapter

Part Number: LP-XDS110ET
Other Parts Discussed in Thread: TMS320F2809

In order to supplement an XSD110 Debug Probe, I'm looking to configure a LP-XDS110ET to be able to flash to and debug a board that takes a standard TI 14-Pin JTAG connector. I tried pairing up the standard JTAG signals (TDI/TCO/TCK/TMS/nRST, plus Vcc and Gnd), and found that I was unable to flash from within Code Composer Studio. I then tried wiring up our existing Debug Probe pin for pin, and found that the board only successfully flashed when EMU0 was connected. Looking at the LP-XDS110ET's 20 pin output, I notice that there are no pins marked as EMU0/1, though we do have 3 GPIO pins and RX/TX lines. Are any of these configured to send out the EMU0 signal? If not by default, can they be made to send the signal?