This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P7: ti-wisunfantund wi-sun networking on BeaglePlay board

Part Number: CC1352P7

I'm trying to get the ti-wisunfantund stack working on a beagleplay dev board. I've been following the instructions from this thread: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1240525/faq-cc1352p7-is-ti-wisunfantund-working-with-the-newly-released-beagleplay-yes?tisearch=e2e-sitesearch&keymatch=faq%3Atrue

I've successfully flashed the NCP with the ns_br firmware and it appears to be working. I'm running into problems with the ns_node. I've successfully compiled and flashed the ncp. I can enable the interface with wfanctl, but I can't enable the stack. when I try with set stack:up true I get this error:

set failed wit error 15335425. NCP-Specific errorcode

Error 15335425 (0xEA001)

  • Hi Lucas, have you also setup the interface with sudo wfanctl set interface:up true prior to set stack:up?

    Regards,

    Arthur

  • Yes, I have done that before enabling the stack.

  • Hi, can you provide any more troubleshooting information for this? The ns_br example seems to work fine, but I'm still stuck on setting up the ns_node.

  • I think that the NCP is starting the stack at the same time as the interface, and that is causing problems. I have limited debugging capability but using the onboard LED I can see that  NcpBase::HandlePropertySet<SPINEL_PROP_NET_STACK_UP>(void) is being called when I don't think it should be.

  • Hi Lucas,

    Difficult to know what could be wrong at this point, but you should indeed definitely wait some amount of time between the call to wfantund, and the interface setup. Right now, it looks like you have no delay between those steps.

    If you had more logs, I could look at them.

    But now, I am wondering, did you set ns_br to autostart the interface? https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1183327/cc1312r7-wi-sun-autostart-bringing-the-network-interface-up-for-embedded-gateways?tisearch=e2e-sitesearch&keymatch=CC1312R7

    Regards,

    Arthur

  • Thanks for getting back to me. Here are the full logs. For this run, I started wfanctl, got the status, set interface:up true, waited for a minute or so, and set stack:up true. Same result as before.

    wfantund[1326]: Starting wfantund 0.08.00d (Feb 13 2024 23:51:12) . . .
    wfantund[1326]:         BUILD_VERSION = 6e0b12f-dirty
    wfantund[1326]: Configuration file "/etc/wpantund.conf" read.
    wfantund[1326]: set-config-param: "Daemon:SyslogMask" set succeded
    wfantund[1326]: Stat (autolog): Tx: 0 packets (0 udp, 0 tcp, 0 icmp6) -- 0 bytes
    wfantund[1326]: Stat (autolog): Tx history is empty
    wfantund[1326]: Stat (autolog):
    wfantund[1326]: Stat (autolog): Rx: 0 packets (0 udp, 0 tcp, 0 icmp6) -- 0 bytes
    wfantund[1326]: Stat (autolog): Rx history is empty
    wfantund[1326]: Stat (autolog):
    wfantund[1326]: Stat (autolog): NCP state history is empty.
    wfantund[1326]: Stat (autolog):
    wfantund[1326]: Stat (autolog):
    wfantund[1326]: Setting baud rate to 115200
    wfantund[1326]: Opening tun interface socket with name "wfan0"
    wfantund[1326]: Getting DBus connection
    wfantund[1326]: Registering DBus connection
    wfantund[1326]: Requesting DBus connection name com.nestlabs.WPANTunnelDriver
    wfantund[1326]: Ready. Using DBUS bus ":1.48"
    wfantund[1326]: Running as root without dropping privileges!
    wfantund[1326]: Initializing NCP
    wfantund[1326]: Removing all NCP originated addresses
    wfantund[1326]: NCP is now BUSY.
    wfantund[1326]: [->NCP] (1) PROP_VALUE_GET(PROTOCOL_VERSION)
    wfantund[1326]: [->NCP] (2) PROP_VALUE_GET(NET_STACK_UP)
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(PROTOCOL_VERSION) [57692D53554E4641...]
    wfantund[1326]: KEY ID: 1
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: State change: "uninitialized" -> "offline"
    wfantund[1326]: [->NCP] (3) PROP_VALUE_GET(PROTOCOL_VERSION)
    wfantund[1326]: [->NCP] (4) PROP_VALUE_GET(NCP_VERSION)
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(PROTOCOL_VERSION) [57692D53554E4641...]
    wfantund[1326]: KEY ID: 1
    wfantund[1326]: [->NCP] (5) PROP_VALUE_GET(INTERFACE_TYPE)
    wfantund[1326]: [->NCP] (6) PROP_VALUE_GET(HWADDR)
    wfantund[1326]: [->NCP] (7) PROP_VALUE_GET(PHY_CCA_THRESHOLD)
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(NCP_VERSION) [5449574953554E46...]
    wfantund[1326]: KEY ID: 2
    wfantund[1326]: NCP is running "TIWISUNFAN/1.0.2; RELEASE; Feb 14 2024 15:33:00"
    wfantund[1326]: Driver is running "0.08.00d (/6e0b12f-dirty; Feb 13 2024 23:51:12)"
    wfantund[1326]: [->NCP] (8) PROP_VALUE_GET(PHY_TX_POWER)
    wfantund[1326]: [->NCP] (9) PROP_VALUE_GET(PHY_REGION)
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(INTERFACE_TYPE) [04]
    wfantund[1326]: KEY ID: 3
    wfantund[1326]: [->NCP] (10) PROP_VALUE_GET(PHY_MODE_ID)
    wfantund[1326]: [->NCP] (11) PROP_VALUE_GET(UNICAST_CHANNEL_LIST)
    wfantund[1326]: [->NCP] (12) PROP_VALUE_GET(BROADCAST_CHANNEL_LIST)
    wfantund[1326]: [->NCP] (13) PROP_VALUE_GET(ASYNC_CHANNEL_LIST)
    wfantund[1326]: [->NCP] (14) PROP_VALUE_GET(CH_SPACING)
    wfantund[1326]: [->NCP] (15) PROP_VALUE_GET(CHO_CENTER_FREQ)
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(NCP_VERSION) [5449574953554E46...]
    wfantund[1326]: KEY ID: 2
    wfantund[1326]: [->NCP] (1) PROP_VALUE_GET(MAC_15_4_PANID)
    wfantund[1326]: [->NCP] (2) PROP_VALUE_GET(UNKNOWN)
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(INTERFACE_TYPE) [04]
    wfantund[1326]: KEY ID: 3
    wfantund[1326]: [->NCP] (3) PROP_VALUE_GET(UNKNOWN)
    wfantund[1326]: [->NCP] (4) PROP_VALUE_GET(UNKNOWN)
    wfantund[1326]: [->NCP] (5) PROP_VALUE_GET(UNKNOWN)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: NCP Status: MACHardwareAddr:   00:12:4B:00:29:C2:D1:91
    wfantund[1326]: [->NCP] (6) PROP_VALUE_GET(UNKNOWN)
    wfantund[1326]: [->NCP] (7) PROP_VALUE_GET(UNKNOWN)
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(PHY_CCA_THRESHOLD) [C4]
    wfantund[1326]: KEY ID: 36
    wfantund[1326]: [->NCP] (8) PROP_VALUE_GET(NET_IF_UP)
    wfantund[1326]: [->NCP] (9) PROP_VALUE_GET(NET_STACK_UP)
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(PHY_TX_POWER) [00]
    wfantund[1326]: KEY ID: 37
    wfantund[1326]: [-NCP-]: Tx power 0
    wfantund[1326]: [->NCP] (10) PROP_VALUE_GET(NET_ROLE)
    wfantund[1326]: [->NCP] (11) PROP_VALUE_GET(NET_NETWORK_NAME)
    wfantund[1326]: Resetting interface(s). . .
    wfantund[1326]: Resetting interface wfan0. . .
    wfantund[1326]: Removing all address/prefix/route entries
    wfantund[1326]: Finished initializing NCP
    wfantund[1326]: property_get_value: key: "NCP:State"
    wfantund[1326]: DBus Sending Interface Added Signal for wfan0
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(PHY_REGION) [01]
    wfantund[1326]: KEY ID: 80
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(PHY_MODE_ID) [02]
    wfantund[1326]: KEY ID: 81
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(UNICAST_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 82
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(BROADCAST_CHANNEL_LIST) [0000000000000000...]
    wfantund[1326]: KEY ID: 83
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(ASYNC_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 84
    wfantund[1326]: [NCP->]: Frame CRC Mismatch: Calc:0xABBF != Frame:0x00C8, Garbage on line?
    wfantund[1326]: [NCP->]: Garbage is not ASCII ([0]=142)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(PHY_CCA_THRESHOLD) [C4]
    wfantund[1326]: KEY ID: 36
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(PHY_TX_POWER) [00]
    wfantund[1326]: KEY ID: 37
    wfantund[1326]: [-NCP-]: Tx power 0
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(PHY_REGION) [01]
    wfantund[1326]: KEY ID: 80
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(PHY_MODE_ID) [02]
    wfantund[1326]: KEY ID: 81
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(UNICAST_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 82
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(BROADCAST_CHANNEL_LIST) [0000000000000000...]
    wfantund[1326]: KEY ID: 83
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(ASYNC_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 84
    wfantund[1326]: [NCP->]: Frame CRC Mismatch: Calc:0xABBF != Frame:0x00C8, Garbage on line?
    wfantund[1326]: [NCP->]: Garbage is not ASCII ([0]=142)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(PHY_CCA_THRESHOLD) [C4]
    wfantund[1326]: KEY ID: 36
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(PHY_TX_POWER) [00]
    wfantund[1326]: KEY ID: 37
    wfantund[1326]: [-NCP-]: Tx power 0
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(PHY_REGION) [01]
    wfantund[1326]: KEY ID: 80
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(PHY_MODE_ID) [02]
    wfantund[1326]: KEY ID: 81
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(UNICAST_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 82
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(BROADCAST_CHANNEL_LIST) [0000000000000000...]
    wfantund[1326]: KEY ID: 83
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(ASYNC_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 84
    wfantund[1326]: [NCP->]: Frame CRC Mismatch: Calc:0xABBF != Frame:0x00C8, Garbage on line?
    wfantund[1326]: [NCP->]: Garbage is not ASCII ([0]=142)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(PHY_CCA_THRESHOLD) [C4]
    wfantund[1326]: KEY ID: 36
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(PHY_TX_POWER) [00]
    wfantund[1326]: KEY ID: 37
    wfantund[1326]: [-NCP-]: Tx power 0
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(PHY_REGION) [01]
    wfantund[1326]: KEY ID: 80
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(PHY_MODE_ID) [02]
    wfantund[1326]: KEY ID: 81
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(UNICAST_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 82
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(BROADCAST_CHANNEL_LIST) [0000000000000000...]
    wfantund[1326]: KEY ID: 83
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(ASYNC_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 84
    wfantund[1326]: [NCP->]: Frame CRC Mismatch: Calc:0xABBF != Frame:0x00C8, Garbage on line?
    wfantund[1326]: [NCP->]: Garbage is not ASCII ([0]=142)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(PHY_CCA_THRESHOLD) [C4]
    wfantund[1326]: KEY ID: 36
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(PHY_TX_POWER) [00]
    wfantund[1326]: KEY ID: 37
    wfantund[1326]: [-NCP-]: Tx power 0
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(PHY_REGION) [01]
    wfantund[1326]: KEY ID: 80
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(PHY_MODE_ID) [02]
    wfantund[1326]: KEY ID: 81
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(UNICAST_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 82
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(BROADCAST_CHANNEL_LIST) [0000000000000000...]
    wfantund[1326]: KEY ID: 83
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(ASYNC_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 84
    wfantund[1326]: [NCP->]: Frame CRC Mismatch: Calc:0xABBF != Frame:0x00C8, Garbage on line?
    wfantund[1326]: [NCP->]: Garbage is not ASCII ([0]=142)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(PHY_CCA_THRESHOLD) [C4]
    wfantund[1326]: KEY ID: 36
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(PHY_TX_POWER) [00]
    wfantund[1326]: KEY ID: 37
    wfantund[1326]: [-NCP-]: Tx power 0
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(PHY_REGION) [01]
    wfantund[1326]: KEY ID: 80
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(PHY_MODE_ID) [02]
    wfantund[1326]: KEY ID: 81
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(UNICAST_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 82
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(BROADCAST_CHANNEL_LIST) [0000000000000000...]
    wfantund[1326]: KEY ID: 83
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(ASYNC_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 84
    wfantund[1326]: [NCP->]: Frame CRC Mismatch: Calc:0xABBF != Frame:0x00C8, Garbage on line?
    wfantund[1326]: [NCP->]: Garbage is not ASCII ([0]=142)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(PHY_CCA_THRESHOLD) [C4]
    wfantund[1326]: KEY ID: 36
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(PHY_TX_POWER) [00]
    wfantund[1326]: KEY ID: 37
    wfantund[1326]: [-NCP-]: Tx power 0
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(PHY_REGION) [01]
    wfantund[1326]: KEY ID: 80
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(PHY_MODE_ID) [02]
    wfantund[1326]: KEY ID: 81
    wfantund[1326]: NCP is no longer busy, host sleep is permitted. (Was busy for 201ms)
    wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Daemon/ReadyForHostSleep - value: true
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(UNICAST_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 82
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(BROADCAST_CHANNEL_LIST) [0000000000000000...]
    wfantund[1326]: KEY ID: 83
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(ASYNC_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 84
    wfantund[1326]: [NCP->]: Frame CRC Mismatch: Calc:0xABBF != Frame:0x00C8, Garbage on line?
    wfantund[1326]: [NCP->]: Garbage is not ASCII ([0]=142)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(PHY_CCA_THRESHOLD) [C4]
    wfantund[1326]: KEY ID: 36
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(PHY_TX_POWER) [00]
    wfantund[1326]: KEY ID: 37
    wfantund[1326]: [-NCP-]: Tx power 0
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(PHY_REGION) [01]
    wfantund[1326]: KEY ID: 80
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(PHY_MODE_ID) [02]
    wfantund[1326]: KEY ID: 81
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(UNICAST_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 82
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(BROADCAST_CHANNEL_LIST) [0000000000000000...]
    wfantund[1326]: KEY ID: 83
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(ASYNC_CHANNEL_LIST) [FFFFFFFFFFFFFFFF...]
    wfantund[1326]: KEY ID: 84
    wfantund[1326]: [NCP->]: Frame CRC Mismatch: Calc:0xABBF != Frame:0x00C8, Garbage on line?
    wfantund[1326]: [NCP->]: Garbage is not ASCII ([0]=142)
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(HWADDR) [00124B0029C2D191]
    wfantund[1326]: KEY ID: 8
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Network/PANID - value: 43981
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: Node type change: "0 : Border Router" -> "sleepy-end-device"
    wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Network/NodeType - value: sleepy-end-device
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Network/Name - value: Wi-SUN Network
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(CHO_CENTER_FREQ) [8603C800]
    wfantund[1326]: KEY ID: 5377
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(CHO_CENTER_FREQ) [8603C800]
    wfantund[1326]: KEY ID: 5377
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(CHO_CENTER_FREQ) [8603C800]
    wfantund[1326]: KEY ID: 5377
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(CHO_CENTER_FREQ) [8603C800]
    wfantund[1326]: KEY ID: 5377
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(CHO_CENTER_FREQ) [8603C800]
    wfantund[1326]: KEY ID: 5377
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(CHO_CENTER_FREQ) [8603C800]
    wfantund[1326]: KEY ID: 5377
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(CHO_CENTER_FREQ) [8603C800]
    wfantund[1326]: KEY ID: 5377
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(CHO_CENTER_FREQ) [8603C800]
    wfantund[1326]: KEY ID: 5377
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(MAC_15_4_PANID) [CDAB]
    wfantund[1326]: KEY ID: 54
    wfantund[1326]: [-NCP-]: PANID 0xABCD
    wfantund[1326]: [NCP->] (2) PROP_VALUE_IS(UNKNOWN) [FF]
    wfantund[1326]: KEY ID: 5462
    wfantund[1326]: [NCP->] (3) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5463
    wfantund[1326]: [NCP->] (4) PROP_VALUE_IS(UNKNOWN) [00000000]
    wfantund[1326]: KEY ID: 5464
    wfantund[1326]: [NCP->] (5) PROP_VALUE_IS(UNKNOWN) [02]
    wfantund[1326]: KEY ID: 5465
    wfantund[1326]: [NCP->] (6) PROP_VALUE_IS(UNKNOWN) [00]
    wfantund[1326]: KEY ID: 5466
    wfantund[1326]: [NCP->] (7) PROP_VALUE_IS(UNKNOWN) []
    wfantund[1326]: KEY ID: 5467
    wfantund[1326]: [NCP->] (8) PROP_VALUE_IS(NET_IF_UP) [00]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is not up
    wfantund[1326]: [NCP->] (9) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: [NCP->] (10) PROP_VALUE_IS(NET_ROLE) [01]
    wfantund[1326]: KEY ID: 67
    wfantund[1326]: [-NCP-]: Net Role "NET_ROLE_CHILD" (1)
    wfantund[1326]: [NCP->] (11) PROP_VALUE_IS(NET_NETWORK_NAME) [57692D53554E204E...]
    wfantund[1326]: KEY ID: 68
    wfantund[1326]: [-NCP-]: Network name "Wi-SUN Network"
    wfantund[1326]: Inbound DBus message for INTERFACE "Status" from ":1.50"
    wfantund[1326]: property_get_value: key: "NCP:State"
    wfantund[1326]: [->NCP] (12) NOOP
    wfantund[1326]: NCP is now BUSY.
    wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Daemon/ReadyForHostSleep - value: false
    wfantund[1326]: [NCP->] (12) PROP_VALUE_IS(LAST_STATUS) [00]
    wfantund[1326]: KEY ID: 0
    wfantund[1326]: [-NCP-]: Last status (OK, 0)
    wfantund[1326]: property_get_value: key: "NCP:State"
    wfantund[1326]: property_get_value: key: "Daemon:Enabled"
    wfantund[1326]: property_get_value: key: "NCP:Version"
    wfantund[1326]: property_get_value: key: "POSIXApp:RCPVersion:Cached"
    wfantund[1326]: property_get_value: key: "Daemon:Version"
    wfantund[1326]: property_get_value: key: "Config:NCP:DriverName"
    wfantund[1326]: property_get_value: key: "NCP:HardwareAddress"
    wfantund[1326]: property_get_value: key: "Network:NodeType"
    wfantund[1326]: property_get_value: key: "Network:PANID"
    wfantund[1326]: NCP is no longer busy, host sleep is permitted. (Was busy for 206ms)wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Daemon/ReadyForHostSleep - value: true
    wfantund[1326]: Inbound DBus message for INTERFACE "PropSet" from ":1.50"
    wfantund[1326]: property_set_value: key: "interface:up"
    wfantund[1326]: [->NCP] (13) PROP_VALUE_SET(NET_IF_UP) [01]
    wfantund[1326]: NCP is now BUSY.
    wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Daemon/ReadyForHostSleep - value: false
    wfantund[1326]: [NCP->] (13) PROP_VALUE_IS(NET_IF_UP) [01]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is up
    wfantund[1326]: [->NCP] (14) PROP_VALUE_SET(NET_STACK_UP) [01]
    wfantund[1326]: [NCP->] (14) PROP_VALUE_IS(NET_STACK_UP) [00]
    wfantund[1326]: KEY ID: 66
    wfantund[1326]: [-NCP-]: Stack is not up
    wfantund[1326]: Sending DBus response for "PropSet" to ":1.50"
    wfantund[1326]: NCP is no longer busy, host sleep is permitted. (Was busy for 209ms)wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Daemon/ReadyForHostSleep - value: true
    wfantund[1326]: Inbound DBus message for INTERFACE "PropSet" from ":1.50"
    wfantund[1326]: property_set_value: key: "stack:up"
    wfantund[1326]: [->NCP] (15) PROP_VALUE_SET(NET_IF_UP) [01]
    wfantund[1326]: NCP is now BUSY.
    wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Daemon/ReadyForHostSleep - value: false
    wfantund[1326]: [NCP->] (15) PROP_VALUE_IS(NET_IF_UP) [01]
    wfantund[1326]: KEY ID: 65
    wfantund[1326]: [-NCP-]: Interface is up
    wfantund[1326]: [->NCP] (1) PROP_VALUE_SET(NET_STACK_UP) [01]
    wfantund[1326]: [NCP->] (1) PROP_VALUE_IS(LAST_STATUS) [01]
    wfantund[1326]: KEY ID: 0
    wfantund[1326]: [-NCP-]: Last status (FAILURE, 1)
    wfantund[1326]: SpinelNCPTaskSendCommand.cpp:351: Requirement Failed ((mRetVal) == 0)
    wfantund[1326]: SendCommand task encountered an error: 15335425 (0x00EA0001)
    wfantund[1326]: Sending DBus response for "PropSet" to ":1.50"
    wfantund[1326]: NCP is no longer busy, host sleep is permitted. (Was busy for 207ms)wfantund[1326]: DBusAPI:PropChanged: /com/nestlabs/WPANTunnelDriver/wfan0/Property/Daemon/ReadyForHostSleep - value: true

    Autostart is not enabled. I haven't changed any of the config from the provided examples.

  • Interestingly, I purchased a LP-CC1352P7-1 dev board, and the ns_node example seems to work only when I am using py-spinel. The interface and stack come up with no problem, and the board connects. It doesn't work with wfantund, though. I get the same issue as I have already described.

  • Hi Lucas,

    It has come to my attention that this is actually a known bug.

    Here is what you should do:

    Current workaround solution:

    1. Apply the following patch to application.c of your ns_node project (/source/ti/ti_wisunfan/apps/udp_nanostack_mesh_tirf/application.c):
      diff --git a/source/ti/ti_wisunfan/apps/udp_nanostack_mesh_tirf/application.c b/source/ti/ti_wisunfan/apps/udp_nanostack_mesh_tirf/application.c
      index 9ea7d79c..79e0c3ad 100644
      --- a/source/ti/ti_wisunfan/apps/udp_nanostack_mesh_tirf/application.c
      +++ b/source/ti/ti_wisunfan/apps/udp_nanostack_mesh_tirf/application.c
      @@ -1628,12 +1628,21 @@ otError nanostack_net_if_up(void)
       /*!
        * Check if the node joined the network or not on starting
        * the connection to network
      - * return value: true if connected, false if not or in the
      - * process of connecting
      + * return value: true if connected or connecting, false if not started
        */
       bool is_net_stack_up(void)
       {
      -    return(connectedFlg);
      +    protocol_interface_info_entry_t *cur;
      +    cur = protocol_stack_interface_info_get(IF_6LoWPAN);
      +    if (!cur) {
      +        return false;
      +    }
      +
      +    if(ER_IDLE != cur->nwk_bootstrap_state)
      +    {
      +        return true;
      +    }
      +    return false;
       }


    2. Flash BR and RN devices. Connect them to two different PC or VMs (there is an network interface issue with having both interfaces on the same host).
    3. Start wfantund and wfanctl as usual on both BR and RN.
    4. Start the BR normally, as specified in the wfantund README.
    5. Start the RN as follows:
      1. Start wfantund and wfanctl
      2. In wfanctl, run ONLY set interface:up true.
      3. Wait until the device is joined. You can verify this by checking the get connecteddevices property on the BR.
      4. Run set stack:up true
    6. You should be able to ping from both BR and RN side now.

    Regards,

    Arthur

  • That seems to fix the issue, thanks!