Part Number: CC110L
Hi,
I am using your CC110L in a design of mine. I am targeting 433MHz. A few questions on the implementation:
1) If I use the helical PCB antenna you used in reference design SWRR081, can I copy the balun and matching component values exactly and expect a perfectly matched antenna? Do I need to tune those values? I think I will always need to retune the matching components due to my PCB shape, case size, and amount of ground plane being different (even if I use the same stack up and board material). Below is the schematic for reference:

2) Do I need to retune the balun values used in reference design SWRR081? Or will those always be correct?
3) How do you figure out what the antenna-matching component values should be? If this was an unbalanced/single ended application, then you could connect a VNA to the transmit signal pad of the IC, measure it, and tune it as necessary. This is a balanced/differential output so I don't think I can use a standard VNA here. Is that correct? Do you have a good application note for taking this measurement?
4) In Application Note AN058, you recommend using Pulse antenna W3127. Is there a reference design for this antenna that uses CC110L part? I'm unsure of what the antenna-matching component values should be. Will the balun values change?
Thanks,
Brandon