Hello,
I have a question regarding OAD (Over-the-Air Device Firmware Update). I am using TI Stack 15.4. During the update of the sensor (CC1310), the update is successful as long as the sensor doesn't lose power/connection. If there is an interruption, the update resumes from where it left off and completes successfully, but the sensor does not reset and boot the new image afterward. Even after a manual reset, the old image is still launched. TIRTOS is stored in flash, so I use "-m 0x1000" when generating the .bin. What could be wrong or what might I be doing incorrectly?
Regards, Ales