Hello everyone,
I have the following problem.
I am working with CC1101 radio, Johanson Technology Balun Matched Filter and use a monopole meander antenna at 915 MHz, figure 1.
Figure1 Meander Antenna
The card was built based on the DN024 and DN025 Design Notes.
Using an RF analyzer to perform measurements on the antenna (figure 2) I have:
· Smith Chart: 48 + j31
· VSWR: 1.8
· Log Mag: -10.3
Figure 2
My design has an Pi network to tune. Being in 48 + J31, my goal is to reach 48 - J21. The theory tells me to place on the PI network a 3.3pF capacitor in series to reach 48 - J21, figure 3.
Figure 3
Nevertheless, in practice the capacitor of 3.3pF has no vertical displacement in the Smith chart, instead it moves to the left: 18 + J1.6, Figure 4.
Figura 4
Q1. Is there some explanation for
this case in which the theory does
not match practice?
Q2. What is the reason for this behavior?
Thanks in advance.
Best regards,
Gregorio