Hi team,
These are from the customer:
I have a need to achieve 1 to 10 node data communication, 1 to the main 10 from
1, the actual effective amount of data from the master to about 5Kbps
2, each node has about 20kbps of actual effective data transferred to the master node, a total of 200kbps
3, requires the entire network to be based on the main implementation time synchronization
4, to achieve frequency hopping function
5, in the complex electromagnetic environment to achieve the actual effective distance of 200m
6, power up 10 seconds to complete all node links across the network
7, currently tentatively use the 433MHZ band, CC1352@20dBm
Q:
1, can be implemented with TI15.4STACK? If not, what ways and ideas can be used?
2, in addition there is no simple data compression algorithm to reduce the amount of data from the main?
Thanks & Best regards,
Yolande