I had been using CC2530 and RF05EB using Windows 7 x64 and had been having intermitent driver issues when downloading and/or debugging.
I was instructed to install the new TI win7 x64 drivers which I did and as far as the OS is concerned these appear to be correct and in order and the devices are connecting and disconnecting fine.
I was advised that to get EW 8051 to recognise the new driver(s) I must install a particular patch OR upgrade to version 8.10.
I upgraded to v8.10 and now the problem seems to have worsened. The driver errors are now consistent rather than intermittent and I have not once managed to load programs or debug.
Does any one have any ideas what I may be doing wrong or may have left out?
Thanks.