This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312PSIP: Can't compile CC1312PSIP TI examples

Part Number: CC1312PSIP


Dear support team,

I'm working with CC1312PSIP controller.

TI RTOS: simplelink_cc13xx_cc26xx_sdk_7_10_02_23

I would like to use this example:

C:\ti\simplelink_cc13xx_cc26xx_sdk_7_10_02_23\examples\rtos\LP_EM_CC1312PSIP\drivers\gpiointerrupt\tirtos7\iar\gpiointerrupt_LP_EM_CC1312PSIP_tirtos7_iar.template.eww

I opened the workspace, than saved it in my local folder.
Got this message:
"The project file gpiointerrupt...PSIP.ewp is an old format. would you like to convert it for use with this version?"   -> YES
"This will open a workspace from a template and save it in a new folder"    -> OK
Save as ... -> SAVE
"Save project "gpiointerrupt_LP_EM_CC1312PSIP_tirtos7_iar?"  ->  YES

After the workspace is saved and opened, an error window popup: "Fatal error while generating source browse information..."

I replaced the Output Browse files to: $_TEMP_$\$PROJ_FNAME$\Debug\BrowseInfo

"Failed to generate browse indexing file"
"Unable to find pbw file"
The project failed to compile.


I'm using IAR version 9.32.1.55115
Shared component version: 9.1.5.10207

Please advice