Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi TI
My CC1352R1 launchpad arrived a few days ago and i was wanting to flash my program into it.
Uniflash came up with the message that the XDS firmware needed updating & proceeded to do it.
It then came up with the message " IcePick_C: Error: (Error -592 @ 0x0) The firmware updater encountered an error and could not finish. The firmware download failed to complete on the XDS110. Unplug and re-plug the XDS110, and try again. If the problem remains, try updating the firmware using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of the installation. View the XDS110SupportReadMe.pdf file there for instructions. (Emulation package 9.10.0.00080)"
on unpluging & repluging power i noticed that the power LED didn't light...plus unflash couldn't see the launchpad (& neither does windows nor XDSDFU).
i then tried the same process on another board that had arrived today...exact same end result!
TWO faulty boards is unlikely so i suspect the issue may be in the process i'm following....is it possible that uniflash left the boards in the DFU state rather than the run state & if so how do i get it back into the run state if the XDSDFU program cant see them???
i am using uniflash 8.2.0 the CCS is 10.4.....
is there anything i can try & if not, who do i contact to get return the board (bearing in mind i'm in New Zealand).
thanks
[update - for others in a similar position] i managed to fix the problem...ground TDO of the XDS110, connected to power, loaded the new firmware!!
see https://software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/emu_xds110.html#troubleshooting
and https://software-dl.ti.com/ccs/esd/documents/ccs_debugging_jtag_connectivity_issues.html
for reference...