Tool/software:
Hello,
I have a system using the CC1125 at two different symbol rates, one about 20x faster than the other.
I have noticed that the SmartRF Studio defaults for the PA Power Ramping Control are the same for all settings of carrier frequency and symbol rate (0 to 1/8 to 11/16 to full power over 3 symbol times).
This means the ramp time for the slow data rate is about 20x slower than for the higher data rate.
As I am using the CC1125 in a battery powered application I would like to reduce the amount of time the RF is on for.
Given I have no EMC issues with the faster data is there any reason why I shouldn't make the slower data rate ramp time faster by dropping the ramp time to 3/8 symbol time and then the slow data rate ramp time will only be 2.5 times slower than the faster data rate?
Thanks,
Ed.