This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R7: Wi-SUN Border Router OAD

Part Number: CC1312R7
Other Parts Discussed in Thread: UNIFLASH

Tool/software:

Hi.

There is a demand from our side to remotely update the WI-SUN Border Router (BR) firmware. Our setup is a BR connected to an embedded Linux gateway. From our tests, the Wi-SUN OAD solution for CoAP Endpoints is not feasible for the Border Router, as the latter does not have enough RAM to run CoAP. With that in mind, the best solution would probably be to direcly flash the firmware through some flash programming tool. Is there an open source flash programming tool which we can use to flash the firmware? It is important for the code to be open source so that  we can compile it to our embedded Linux gateway.

Besides, we are open suggestions other than the flash programming tool.

Regards,

Mauricio.