This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530 based Node Lifetime

Other Parts Discussed in Thread: CC2530

Hi,

I am designing a Node using CC2530 which needs battery lifetime of 2 years and powered by 950maH coin cell battery.

My expected range of communication is 1-20 meter.

It is using Zstack with Key event triggered and Timer triggered mode.

Key Event rate is 10 event/Day.Which will be generated by Key pressed condition(3 GPIO Key is in use).As soon as key event is triggered, It will try to connect with Coordinator.It will use transmit power such that 20 meter range can be achieved.

Once End Device is in connection with Coordinator, It will use Timer triggered mode in which after every 10 second it will send Keep Alive Message.Maximum time for which Timer trigger can run is 10 hour/Day.

Can anyone suggest some real world example which is using CC2530 and carried out some kind of analysis.

How much difference it can make if Use SimpliTI stack instead of Zigbee Stack. I don't need capability of Zigbee protocol.

Is there any kind of Power consumption/Battery life analysis done by TI/Community member?

Is it possible at all.?2 year life time?

I am using

3 GPIO(Just for 10 event a day)

10 event/Day(Deep Sleep)

10 second timer trigger event for 10 hours/day(Timer Sleep)