Tool/software:
I am using CC1312R to develop products using 920MHz and 1200MHz frequencies.
However, the overall noise floor at 920 MHz is high and spurious around the carrier wave does not meet the standard.
The 1200 MHz band also fails to meet spurious standards in the neighboring bands.
Although IIR filters, PLLs, etc. are being studied by changing values from registers, it is necessary to sacrifice ACP in order to meet the spurious standard, and the situation is such that only one of the two standards, either spurious or ACP, can be met.
[QUESTIONS]
・The CC1312R itself seems to have a higher noise floor overall, but is this what this RFIC is like?
・Since the noise floor around the carrier wave is high, is there any way to set up a filter or register that can drop spurious in this area?