This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello I have a CC1101 device I am integrating with that uses synchronous serial mode. I have input the supplied parameters for the CC1101 in Smart RF studio as seen in the picture. I have connected the pins to my logic analyzer and I see lots of random data on GDO2 as soon as the clock starts with no intentional data being transmitted. In continuous RX mode I can see a RSSI spike in the output showing that the data is sent but I can not get the data because of the random GDO2 output. I am expecting a 0xF0 preamble sequence but so far have been unable to get that. I get the same results on the custom development board I set up as well. Any help would be apreciated.
Ok I think this might be because the modules i purchased online are 433mhz antenna configuration so I am going to say that is likely a problem
I will close this case then, and then you can reopen it if you still have problems when operating ont he correct frequency with the correct antennas, for the CC1101EM version that you have.
SIri