Tool/software:
Sorry for the series of threads.
Regarding the frequency deviation, we recognise that the problem is that there is a frequency deviation between the L, M and H channels in the same frequency band, and we are not asking whether each channel meets the standard or not.
Essentially, the frequency deviation depends on the reference frequency of the oscillator etc. and is considered to be approximately equal at L, M and H. If the frequency deviation is different for L, M and H, it will be difficult to incorporate the frequency deviation into the product.
In case you are wondering, a TCXO was used as the reference clock and the frequency deviation was about +0.43 ppm.
Is there any solution to this?
regards.