Part Number: CC1352P7
Other Parts Discussed in Thread: SYSBIOS
Tool/software:
Hello,
I am developing a proprietary RF network, and am currently using the following SDK "simplelink_cc13xx_cc26xx_sdk_7_10_01_24". My firmware keeps hitting a Hard Fault caused by the INVSTATE fault from the ARM core. Looking at the ROV I see the following exception information.


Looking at the LR register it appears to trace back to the ti_sysbios_knl_Swi_post function as shown.

I want to try an trace this farther, but the HWI: Exception Call Stack is not giving any information. I am not sure why this is happening. You can see the error in the following image.

If you have some information as to why this error is occurring and any ideas as to what could be checked to help narrow down this problem, it would be appreciated.
Best,
Josh