This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC1311P3: CC1311 RF power problem, how to change the frequency channel and how to wake up the standby

Part Number: LP-CC1311P3
Other Parts Discussed in Thread: CC1311P3

Tool/software:

Hello

I have 3 questions for CC1311 RF.

1.How to change the RF channel?

    For example: channel 0 = 868MHz at the beginning, and every 200kHz is 1 channel, so channel 1 = 868.2MHz

                          CMD_FS is set to the starting frequency of 868MHz. How to change the channel later?

2. How to replace RF power with TX power?

    txpower's IB, GC, boost, tempCoeff, how to adjust these four parameters?

    I want the tx power to be 8.5dBm: IB, GC, boost, tempCoeff. How to adjust these four parameters?

    For example: in the example -11dBm => 2, 3, 0, 7, how do these four values ​​come out?

    I want to adjust to 5.4dBm. How do I adjust these four values?

3.CC1311 enters standby mode: Power_sleep(PowerCC26XX_STANDBY); How to use RCOSC_LF to wake up?