Other Parts Discussed in Thread: LP-XDS110ET, CC1312R,
Tool/software:
Hi Ti experts.
We have CC1312 and CC1314 chips in the same module, using the LP-XDS110ET development kit debugger, smart rf studio7
With the same settings, replace the chip and test 1250MHz.
The following are CC1312R smart rf studio7 settings

The following is the CC1312 TX power..
We set 13dbm, and the actual measurement was about 10.96dBm, so far so good.

Next, we replace the chip of the CC1312 module just now with CC1314R10 and use smart rf studio7 to set it up

When we replace the CC1312 chip with CC1314, its tx power will become about -13dbm.

so How can we solve this problem?
Thx.