Tool/software:
Can I get a list of the version for Wireshark and the SmartRF packet sniffer that work together and if the set of instructions for setting up to sniff the packets for the sensor/collector project are what is in Getting Started — SmartRF Packet Sniffer 2 User Guide documentation? I had Wireshark reload and now I can't get the setup for it to work. Also, will it decode the data packets? Looking through the data using a generic protocol it looks like it is using UDP with a source and destination address of 192.168.1.3 and ports of 17757, is this correct? I also don't see where the PANID would be is that in the data? I need it to work with the 802.15.4 protocol and the Non Beacon 5kbps SimpleLink PHY.
Thank you,
Kevin