This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: SPI transfer

Part Number: CC1312R


Tool/software:

Hi,

Some SPI sensors have the "nasty" feature of holding the MISO(POCI) pin low while they process a message.

e.g. TSYS01 from TE connectivity.

This is not according to the SPI standard, but we have to work with it.
***

How will the SPI drivers in simplelink SDK handle this.

Will they not return/finish until the MISO pin goes high?
I assume the option is to poll the MISO pin, but can this be done while it is configured a SPI peripheral?

Or do we have to re-configure to GPIO, poll the MISO line a reconfigure to SPI afterwards?

-no_more_wires