This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312PSIP: Energy Detect scan in Sensor/Collector project

Part Number: CC1312PSIP


Tool/software:

I was debugging through code for the sensor/collector project and found that the energy detect scan is not coming back with any scan values.  It is setup without a network since when devices are paired it just uses the stored channel value.  What I see is that the channels to be scanned is set to 1 and it calls scanCnfCb(ApiMac_mlmeScanCnf_t *pData) and gets to the ApiMac_scantype_active check which is when it looks for the energyDetect values and pData->resultListSize is 0.

The original question was:

We are needing to verify that the energy detection for picking a channel is working.  This will let us know if a channel is busy that it won’t be picked as the active channel for communication.

We are thinking we can busy out a set of frequencies using Smart RF Studio by sending data to those frequencies at a rapid pace and then check if the application picks a freq. outside of the busy frequencies.

When I was testing this, it seemed to still pick the same first frequency that it would normally choose.

Can you indicate if this should work or what a valid test would be for this so we can verify this functionality of the protocol?

After debugging the code trying to at least see what values I could get, I can't see any values coming back from the scanning.

Thanks,

Kevin