This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1314R10: Maximum bitrate

Part Number: CC1314R10


Tool/software:

From table 8.1, Feature support I find that both 2(g)fsk and 4(g)fsk are supported, and that the highest sample speed is <= 2 Msps

Is there any example of setting up the radio for 4 Mbps, which I guess is the maximum?

Preferably in proprietary mode.....

Best Regards,

Gullik