Tool/software:
We found that the CC1310F128 has a probability of burning the chip when it is programming with 3.3V battery (the burning tool is the 1310 development board). . The performance phenomenon is that the positive and negative electrodes of the chip are short circuit, the current is more than 100 mA, and the chip is hot, but the product functions normally.
I consulted in the Chinese forum, and the suggestion was to disconnect the 3.3V of the burner, but it didn't work.
More than 20 out of 8,000 were found to be in this condition. I have also encountered a sudden short circuit of the chip in the process of hanging up. We are worried that similar things will happen during the operation of the product, and we hope to know the root cause of this problem.