This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: Reset pin

Part Number: CC1200


Tool/software:

Hi

-. Is there a PULL DOWN resistance inside the CC1200 RESET pin?
-. If there is a PULL DOWN resistance, should it be controlled from GPIO to HIGH in MCU? (HIGH hold time?)

Thanks

  • Hi David,

    The CC1200 does not have internal pull up or pull down on the reset pin. The pin should be driven by a GPIO of an external MCU or tied to VDD.

    The device is reset when the reset pin is pulled low and should be held high during operation.