This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1354P10: IPC Schematic for 20 dBm PA

Part Number: CC1354P10


Tool/software:

Hello.

A circuit using an IPC 0900PC15A0043  for 20 dBm PA. Can you tell me what frequency the 20 dBm output is set to?

In the datasheet on the IPC reference schematic slightly different inductance and capacitance values. It also doesn't say what frequency the output is set to.

I want to set the output to 20 dBm at 868 MHz.  Are these components suitable for this frequency?

Thanks for the reply.

  • Hi,

    At the time of writing, using the Johanson 0900PC15D0043001E Sub-1 GHz, +20 dBm IPC the recommended matching network is:

    L332 10 nH
    C11 1.2 pF

    The PA table setting 0x3F00FF is recommended in order to meet regulatory requirements at 868 MHz (and 915 MHz) for +20 dBm TX output power.

    We will be updating the available information for the +20 dBm IPCs but cannot give a timeframe for this on E2E.

    Regards,

    Zack