Tool/software:
Hi Champs:
Some questions :
Q1. How is the CC13 reset pin + DIO15 pin connection when you are doing UART download from the Processor?
Q2. The DIO15 pin needs to GND all the time during the download period?
Please see the below pic, what is the action we need to perform regarding the DIO15 and Reset pin?
Case1: Do we need to short the (DIO15 to GND) + (Reset pin) all the time till download finished?
Case2: Do we need to short the (DIO15 to GND) only all the time till download finished?
Case3: Do we need to short the (Reset pin) all the time till download finished? ß I don’t think so.
Q3. And we only do reset before the download?
Q4. May you show me how is your HW connection design of this part?
Q5. Do you have the SBL success download log?
plz do help for this urgent case.
Thanks.
BR Rio