CC1310: SimpleLink SDK: CC13x0 v4.20.02.07 vs. CC13xx CC26xx v7.41.00.17

Part Number: CC1310

Tool/software:

Hi there,

The CC1310 product page lists the CC13x0 SDK as the correct one to use:

https://www.ti.com/product/CC1310#software-development

But there is also a much newer CC13xx CC26xx SDK available. Which one is the correct one to use for the CC1310 and why? It seems that support for the CC13x0 SDK has stopped? Would I benefit from bug fixes if I switch to the CC13xx CC26xx SDK?

Thanks in advance,

Pieter

  • Hi Pieter,

    The CC13x0 is supported, and the SDK that you should use is indeed the CC13x0  SDK v4.20.02.07 (LOWPOWER-F1).

    You will not be able to use the LOWPOWER-F2 SDK on the CC13x0 as it is made for the later generation of devices.

    Regards,

    Arthur