Other Parts Discussed in Thread: CC1314R10, SYSCONFIG,
Tool/software:
Good evening,
i'm Luca Gandolfi and i have a problem with CCS12.8.1 and simplelink_cc13xx_cc26xx_sdk_7_41_00_17, when i use CC1314R10.
In particular, the SysConfig configurator have a layout problem thta allows me to use only one SubGhz physical layer (PHY 868MHz) .
I would also need to use the 433MHz PHY, which instead i can do for example if i use the CC1312.
This appears to be due to the RF Design relating to the CC1314 which does not allow the physical layer (PHY 433MHz) to be configured.
Do you have an idea on how i can solve the problem??
Best Regards,
Luca Gandolfi
VA.RE.L s.r.l.
Via Dell'Artigianato, 18
26029 SONCINO (CR) ITALY
Tel. +39 (0)374 83141
www.varel.it
l.gandolfi@varel.it