Tool/software:
Everyone,
I’m currently working on a project using the CC1310 platform and need to implement a Wireless M-Bus (EN 13757-4) communication link. However, I’d prefer not to license the third-party stack from Stackforce at this stage due to budget and integration considerations. Need to achieve full or near-full Wireless M-Bus compliance (S-mode, T-mode, or whichever is needed). CC1310 LaunchPad with the standard smartrf_settings for 868 MHz.
- Are there any open-source or community-driven Wireless M-Bus implementations available for TI CC13xx devices?
- Does TI provide any reference projects or partial examples in Resource Explorer or App Notes that could be adapted into a Wireless M-Bus solution?
- Has anyone successfully rolled out their own custom Wireless M-Bus stack on CC13xx without Stackforce or Radiocrafts modules?
I appreciate any guidance, example code links, or personal experiences you can share. Thank you in advance!