This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2674P10: DC/DC to Global LDO dynamic switch

Part Number: CC2674P10

Tool/software:

Hi, 

Based on the doc online - when using the internal DCDC, VDDR should be 1.68 V to 1.95 V when VDDS > 2.0V. If VDDS < 2.0 V; then it will switch automatically from DCDC Converter Mode to Global LDO Mode.

One question - when using the internal DCDC, if the inductor Lddc has an issue (so let's assume DCDC_SW is floating) VDDS should remain > 2V but VDDR should go down to 0. Do you confirm there is saety mecanism which switches dynamically in Global LDO mode to maintain 1.64V on VDDR ?

Regards,

Geoffrey