This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1354P10: CC1354P10 issue with XDS110 3.0.0.36 firmware

Part Number: CC1354P10

Tool/software:

I updated to CCS 20.1.0 which included XDS110 3.0.0.36. After updating the XDS firmware I receive the following error when debugging (or flashing)

File Loader: Memory write failed:   Status 0x00201400: Target flashloader has not returned any status. Unknown error! GEL: File: C:\Users\xxxxxx\AppData\Local\Temp\ti_cloud_storage\portable_LP_EM_CC1354P10_1_tirtos7_ticlang.out: Load failed.

If I downgrade using the xdsdfu to v3.0.0.35 then the program works again.

c:\ti\ccs2002\ccs\ccs_base\common\uscif\xds110> .\xdsdfu.exe -f firmware_3.0.0.35.bin -r